IV and CV Offline Mode (formerly Demo Mode)
The host PC does not need to be connected to any test equipment hardware to run the demonstration plots (Offline Mode). The Offline Mode provides sample characterization plots of FET and IGBT devices and a test result (*.mdm) file.
IV and CV Offline Mode
Although the demo runs without any test equipment attached to the host PC, you must provide a slot address for each SMU in the Hardware Configuration dialog.
- 
                                                To run the PD1000A IV and CV demonstration, check the Offline Mode checkbox on the display screen. 
- 
                                                Select one or more tests for demonstration plots. If you select multiple tests, the demos run sequentially. 
- 
                                                Click the  button at the bottom of the screen. If you selected more than one test, the data display area changes to show the different test that is running. button at the bottom of the screen. If you selected more than one test, the data display area changes to show the different test that is running.  
- 
                                                Click  to run the demonstration program again. to run the demonstration program again.